Skip to main content
UpStream
Associate
Mar 27, 2023 2:01 AM UTC
Question

Interrupts in EEPROM emulation(AN3969)

I'm trying to implement "AN3969 EEPROM emulation in STM32F40x/STM32F41x microcontrollers" on STM32F407.

According to the documentation, "Interrupt servicing during program/erase is possible".

However, when actually installed, interrupts stop completely during the erase time.

What is the way around this?

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Mar 27, 2023 3:05 AM UTC

It's an MCU not MPU, I fixed the tagging

If the ALL code / vectors / interrupts are all in RAM it might not stall. The erase or write of the Flash will block attempts to concurrently read from Flash.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
Mar 28, 2023 12:40 PM UTC

Hello @UpStream​,

Additionally, it is possible to relocate the interrupt vectors to a different bank of flash or some place in the user Flash memory that is not affected by the program/erase operation maybe temporarily to ensure uninterrupted interrupt service routine.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
UpStream
UpStreamAuthor
Associate
Mar 29, 2023 8:11 AM UTC

Thanks for the reply.

The EEPROM is using the default values sector 2 and sector 3.

The interrupt vector is also set to the initial value, sector 0. Is this a problem?

​

I am testing by porting "eeprom.c" to the sample code "TIM_TimeBase" using STM32F4DISCOVERY Discovery kit.

I moved most of the functions to RAM, but there is no improvement at all.

The move to RAM is

​

Edit STM32F407VGTx_FLASH.ld

----​

_sidata = LOADADDR(.data);

.data :

{

. = ALIGN(8);

_sdata = .;

*(.data)

*(.data*)

*(.code_in_ram) <--- Insert

. = ALIGN(4);

_edata = .;

} >RAM AT> FLASH

​----

​

Add to my code

----​

__attribute__ ((long_call, section (".code_in_ram"))) void foo(void)               

{                                         

 // Do something here

}

----​

I used

​

Is there any help for me ?​

UpStream
UpStreamAuthor
Associate
Mar 30, 2023 9:24 AM UTC

Thank you always for your cooperation. 

After that.

Interrupt vectors could also be switched to SRAM, but interrupts stop during Flash erase.

Am I still missing something?

​

// STM32F407VGTx_FLASH.ld //

/* Specify the memory areas */

MEMORY

{

  RAM_BOOT (xrw)     : ORIGIN = 0x20000000, LENGTH = 8K <--- Insert

  RAM (xrw)        : ORIGIN = 0x20002000, LENGTH = 120K

  CCMRAM (xrw)      : ORIGIN = 0x10000000, LENGTH = 64K

  FLASH_BOOT (rx)     : ORIGIN = 0x8000000,

               LENGTH = 32k

  EMULATED_EEPROM (rwx)  : ORIGIN = ORIGIN(FLASH_BOOT) + LENGTH(FLASH_BOOT), 

               LENGTH = 32k

FLASH (rx)       : ORIGIN = ORIGIN(EMULATED_EEPROM) + LENGTH(EMULATED_EEPROM),

               LENGTH = 1024k - LENGTH(FLASH_BOOT) - LENGTH(EMULATED_EEPROM)

}

​

// system_stm32f4xx.c //

​void SystemInit(void)

{

..........​

​ /* Disable all interrupts */

 RCC->CIR = 0x00000000;

​

 memcpy((void*)0x20000000,(void const*)0x08000000,0x1FFF); <--- Insert

​

 /* Configure the Vector Table location add offset address ------------------*/

#ifdef VECT_TAB_SRAM <-- Select define

 SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */

#else

 SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */

#endif

}