Skip to main content
VChav.19
Associate II
May 8, 2019 1:01 PM UTC
Question

(Interrupt fault handler for flash is called when using x-cube-eeprom example

Im using the X-CUBE-EEPROM to simluate an eeprom with the flash for a nucleo development board (NUCLEO-L452RE-P).

When adapting the example and debugging it, the HardFault_Handler routine from EEPROM_Emul/STM32L4/Src/stm32l4xx_it.c is called when the routine "EE_Init" is called at the main.c file.

Im using Atollic TrueStudio and imported the project from this directory:

\Projects\Multi\Applications\EEPROM_Emul\STM32L4\EWARM\STM32L4R5ZI_Nucleo

Is there any extra configuration I have to set for it to work?

This topic has been closed for replies.