Skip to main content
Associate II
September 25, 2025
Question

Intergrate littlefs file system for stm32h753 in stm32cubeide

Trying to store some ssl certificates and device configurations in STM32h753zi internal flash using littlefs file system https://github.com/littlefs-project/littlefs. but i could not able find any example in there. i anyone had experience in stm32h7(2MB, 2bank) flash read/write operations with wear leveling. any examples or further guidance could be helpfull. im fine with any effective solutions (not bounded to littlefs).

This topic has been closed for replies.

5 replies

mƎALLEm
ST Technical Moderator
September 25, 2025

Hello,

Unfortunately, ST doesn't provide LittleFS implementation. You may need to look for some implementations on the internet.

See the examples provided by @hans86 in this thread based on STM32H743 device.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
September 25, 2025

That GitHub page says, "Detailed documentation (or at least as much detail as is currently available) can be found in the comments in lfs.h." - so have you looked at that?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
EmaticAuthor
Associate II
September 25, 2025

@Andrew Neil there is documentation about how their functions works, not about interfacing between stm32h7 memory.

Pavel A.
September 26, 2025

Why do you want any filesystem at all? It is easier just to include a file or few files into the image, like the "filesystem" used in the http server examples; or burn them into free space on the flash at known addresses.