Skip to main content
Associate
Oct 7, 2025 11:26 AM UTC
Question

Interface STM32L4 MCU with BLUENRG-M2SA Module via SPI

Hello ST Community,

I’m currently working on a project where I’m using the STM32L475RGT6 MCU to interface with the BlueNRG-M2SA Bluetooth module via SPI. The goal is to establish BLE communication between the MCU and a mobile device. However, I’ve encountered a few challenges and would appreciate guidance or reference material.

If anyone has:

  • A working DTM firmware or BLE SPI reference for STM32L4 + BlueNRG-M2SA
  • A minimal working .ioc + main.c + app_bluenrg_2.c
  • Any tips on pin configuration, middleware integration, or BLE stack setup
This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
Oct 9, 2025 3:51 PM UTC

Hello @Muyeez and welcome to the community;

 

May be these ressources can help you:

KDJEM1_0-1760024825240.png

You can find in the readme file the used pins for SPI:
- CS: DIO11
- MISO: DIO2
- MOSI: DIO3
- CLCK: DIO0
- IRQ: DIO7

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
MuyeezAuthor
Associate
Oct 10, 2025 5:20 AM UTC

- CS: DIO11
- MISO: DIO2
- MOSI: DIO3
- CLCK: DIO0
- IRQ: DIO7 

i wanted to know the proper spi file which can make the module advertise and communicate with stm32l475rgt6 and it is a custom board. i have attached the schematic too in which i wanted to know is it correct if correct what could be the fault that im not able to communicate