Associate III
Apr 11, 2019 12:10 PM UTC
Question
Input Capture Mode- STM32 MAT Target
- 0 replies
- 849 views
Hello everybody,
I want to measure the duty Cycle of a PWM Signal in Simulink. . I have managed it to generate a PWM signal with Simulink and STM32 MAT-Target. The problem is now when build a simple model to generate the code, the lines between the blocks will turn to red. and thus i am not able to measure the duty cycle with input capture direct mode. Can someone help with this?
BR
#Pwm-input-capture #Simulink #PWM #[STM32-Mat/Target] #Matlab #TIMER #