Skip to main content
subu.rama
Associate II
Apr 13, 2019 12:00 PM UTC
Solved

Infinite loop in HAL_RCC_GetSysClockFreq() in HAL_RCC_ClockConfig() onNucleo STM32F446RE

I am using the latest System Workbench on Nucleo to set up for experiments.

My code is as follows:

#define SYS_CLOCK_FREQ_50_MHZ 50
 
int main(void)
{
 
	HAL_Init();
 
 
	SystemClock_Config_HSE(SYS_CLOCK_FREQ_50_MHZ);
 
	GPIO_Init();
 
	UART2_Init();
 
	TIMER2_Init();
...

The SystemClock_Config_HSE(...) is as follows:

void SystemClock_Config_HSE(uint8_t clock_freq)
{
	RCC_OscInitTypeDef Osc_Init;
	RCC_ClkInitTypeDef Clock_Init;
 uint8_t flash_latency=0;
 
	Osc_Init.OscillatorType = RCC_OSCILLATORTYPE_HSE | RCC_OSCILLATORTYPE_LSE | RCC_OSCILLATORTYPE_HSI ;
	Osc_Init.HSEState = RCC_HSE_ON;
	Osc_Init.LSEState = RCC_LSE_ON;
	Osc_Init.HSIState = RCC_HSI_ON;
	Osc_Init.PLL.PLLState = RCC_PLL_ON;
	Osc_Init.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 
	switch(clock_freq)
	 {
	 case SYS_CLOCK_FREQ_50_MHZ:
		 Osc_Init.PLL.PLLM = 4;
		 Osc_Init.PLL.PLLN = 50;
		 Osc_Init.PLL.PLLP = RCC_PLLP_DIV2;
		 Osc_Init.PLL.PLLQ = 2;
		 Osc_Init.PLL.PLLR = 2;
		 Clock_Init.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
	 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
		 Clock_Init.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
		 Clock_Init.AHBCLKDivider = RCC_SYSCLK_DIV1;
		 Clock_Init.APB1CLKDivider = RCC_HCLK_DIV2;
		 Clock_Init.APB2CLKDivider = RCC_HCLK_DIV1;
 flash_latency = 1;
	 break;
 
	 case SYS_CLOCK_FREQ_84_MHZ:
		<< These cases are not relevant here>>
	 default:
	 return ;
	 }
 
		if (HAL_RCC_OscConfig(&Osc_Init) != HAL_OK)
	{
			Error_handler();
	}
 
 
 
	if (HAL_RCC_ClockConfig(&Clock_Init, flash_latency) != HAL_OK)
	{
		Error_handler();
	}
 
 
	/*Configure the systick timer interrupt frequency (for every 1 ms) */
	uint32_t hclk_freq = HAL_RCC_GetHCLKFreq();
	HAL_SYSTICK_Config(hclk_freq/1000);
 
	/**Configure the Systick
	*/
	HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
	/* SysTick_IRQn interrupt configuration */
	HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
 
 }

Now when I build, load the program and try running it in the debugger I see that it is stuck in an infinite loop in HAL_RCC_ClockConfig(...). Why did it go into the WWDG_IRQHandler()?

0690X000008AUbFQAW.jpg

This EXACT same code runs fine under Keil MDK.

The version of System Workbench I am using is:

0690X000008AUbKQAW.jpg

Any ideas? I tried it with a previous version of System Workbench and I have the same issue.

Thank you

Subu

This topic has been closed for replies.
subu.rama
subu.ramaBest answer
Associate II
Apr 13, 2019 12:26 PM UTC

Found out the this project was using an older version of the firmware package.

CubeMX was initially used to generate a skeleton/template and code was modified to be as shown above.

0690X000008AUcXQAW.jpg

Once the project was redone using the latest CubeMX firmware, it all worked as it should.

Sorry for the noise on this forum.

Thank you

Subu

1 reply

subu.rama
subu.ramaAuthorBest answer
Associate II
Apr 13, 2019 12:26 PM UTC

Found out the this project was using an older version of the firmware package.

CubeMX was initially used to generate a skeleton/template and code was modified to be as shown above.

0690X000008AUcXQAW.jpg

Once the project was redone using the latest CubeMX firmware, it all worked as it should.

Sorry for the noise on this forum.

Thank you

Subu