Skip to main content
Visitor II
Dec 9, 2025 2:13 PM UTC
Question

i2c for x_nucleo_53l8a1 and stm32H7 Nucleo board.

I was trying to use the xcube_TOF application inside the st32cubemx for the stm32h7 nucleo board. However, the tof initialisation is keep getting failed. 
Is it really possible to implement a i2c connection between x_nucleo_53l8a1 and the stm32H7 nucleo board? 
I tried to implement the hardware connections just like in the stm32nucleof401re.
Could anyone please help me with this?

1 reply

ST Technical Moderator
Jun 26, 2026 4:42 PM UTC

Hi ​@karthii 

You should refer to the user manual Getting started with the X-NUCLEO-53L8A1 Time-of-Flight expansion board based on the VL53L8 series for STM32 Nucleo - User manual

  • I2C integration is possible on the X-NUCLEO-53L8A1 with STM32H7 Nucleo at hardware level
  • The board must be stacked on a Nucleo with Arduino R3 connectors
  • Set J9 to I2C mode : pins 2–3 connected
  • The examples are designed for NUCLEO-F401RE only, so on STM32H7 you need to integrate and adapt the project manually

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL