Skip to main content
Stastny.Petr
Associate III
Jun 7, 2022 8:55 AM UTC
Question

I have STM32G030J6 with 32kB Flash and I need emulate EEPROM. Is it possible?

I need permanently save configuration data (several bytes only) in STM32G030J6 in SO8N package. I tried to use EEPROM emulation SW but not working - very robust and complicated. Is there some easy way how to do this? There is no other EEPROM and no possible to connect.

This topic has been closed for replies.

14 replies

Peter BENSCH
ST Technical Moderator
Jun 19, 2022 8:50 AM UTC
The suggestion of @ne562 is a good idea, but the guaranteed write cycle endurance of the STM32G030 is 1000 cycles - guaranteed over the entire temperature range! Of course higher numbers can be achieved in restricted temperature ranges and especially at lower temperatures, but this is not part of the respective data sheet.
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ne562
Associate III
Jun 19, 2022 9:10 AM UTC

I agree, at extreme temperatures (over 80..100deg.C) number of cycles can be significantly lower (leakage current increases exponentially).

I tested at 22deg and 60deg - no detectable difference, in my applications MCU rarely heats over 40deg...