I am using DWM1000 on a board with a microcontroller STM32L431CC. I am facing a strange issue when the battery becomes weak and can’t provide the power needed for DWM1000 initialization.
- 6 replies
- 2422 views
Hello,
I am using DWM1000 on a board with a microcontroller STM32L431CC. I am facing a strange issue when the battery becomes weak and can’t provide the power needed for DWM1000 initialization.
When the battery is too weak, the board resets because of DWM1000 initialization. After a random number of attemps, the microcontroller does not start anymore. At this point, i am not able to do anything with my board, it is like the code have been erased or the microcontroller is locked in a strange state. Even after disconnecting the battery or connecting a new one, it doesn’t start again. The only way to make it work again is to reflash the board.
I can avoid this problem by putting a 500ms delay before DWM1000 initialization when my boards resets, but i would like to know if this is a known issue ? Is it possible that STM32L431CC locks or loses the code ?
Here you can see the power voltage applied with the weak battery. At the first three attempts of connecting the battery, the battery is too weak to initialize DWM1000. At the fourth attempt, the code has kind of disappeared…