Skip to main content
rtursen
Associate III
Jan 23, 2019 6:28 PM UTC
Question

How to sync trueStudio settings?

Here is the situation, there are 2 developers. Both developers download the code from the repository and issue a build & debug cycle.

Test_functions is an array of function pointers. In the debug session, Test_functions has different values (given in below pictures)

Note Test_15_ArmTest section is normal

0690X000006DDSAQA4.png

Note that in below picture, Test_15_ArmTest section has a "+2 " added to it for some reason and the application doesn't work

0690X000006DDSFQA4.png

I think this has to do with the project properties but I wasn't able to find the cause of the problem. I tried disabling optimizations and disable dead code, dead data removal but the problem persists.

Can you please guide me about this?

ps: test_functions is defined as below

#define TEST_FUNC_ARRAY() \
 test_function_t test_functions[TestDef__Max_] = { \
 &Test_ST1_Bit, \
 &Test_ST2_Bit, \
 &Test_1_PowerUp, \
 &Test_2_HighVoltForPol, \
 &Test_3_HighVoltForPol, \
 &Test_4_HighVoltForPol, \
 &Test_5_HighVoltRevPol, \
 &Test_6_HighVoltRevPol, \
 &Test_7_MCUprogram, \
 &Test_8_InitialSetup, \
 &Test_9_InitialSetup, \
 &Test_10_InitialSetup, \
 &Test_11_InitialSetup, \
 &Test_12_InitialSetup, \
 &Test_13_InitialSetup, \
 &Test_14_TargetClock, \
 &Test_15_ArmTest, \
 &Test_16_InvalidCommand, \
 &Test_17_ClearStatus, \
 ...

This topic has been closed for replies.