Skip to main content
SDel.19
Associate II
Jul 24, 2019 1:45 AM UTC
Question

How to read and storage data on an I2C eeprom using an stm32f100 series board.

Hello, I' m working in team on a project using stm32 f100 series board. I should use an eeprom to storage and read some data, the eeprom is the following: CAT24C512WI-GT3 and I also have the init code for this I2C eeprom:

void io_ee_scl(char s)
{
	if(s)
		GPIOB->BSRR=GPIO_PIN_6;
	else
		GPIOB->BRR=GPIO_PIN_6;
}
 
void io_ee_sda(char s)
{
	if(s)
		GPIOB->BSRR=GPIO_PIN_7;
	else
		GPIOB->BRR=GPIO_PIN_7;
 
}
 
void io_ee_wp(char s)
{
	if(s)
		GPIOB->BSRR=GPIO_PIN_5;
	else
		GPIOB->BRR=GPIO_PIN_5;
}
char read_eeprom() //read eeprom function
{
	return ( (GPIOB->IDR&GPIO_PIN_7) ? 1 : 0 );
}

so I know the pins conected to my eeprom.

Considering I'm new in stm32 I need your help to understand how I can read and write datas on my eeprom....

Thank you

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Jul 24, 2019 2:35 AM UTC

So you're bit-bang it and not using the I2C peripheral?

Here's the manual for your device http://www.onsemi.com/pub/Collateral/CAT24C512-D.PDF

It describes the signals on the I2C pins, and how the address (eeprom) and data are sent.

Perhaps you can extend your code to implement the functionality described?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SDel.19
SDel.19Author
Associate II
Aug 17, 2019 1:59 AM UTC

Yes I am bit banging, can you suggest me where to find c code for do it?

SDel.19
SDel.19Author
Associate II
Aug 17, 2019 1:58 AM UTC

Yes I am bit banging, can you suggest me where to find c code for do it?

S.Ma
Principal
Aug 17, 2019 6:33 AM UTC

I have shared in this forum an example of I2C bit banging with EEPROM simple customizable source code.

Now, use the forum to find it.

SDel.19
SDel.19Author
Associate II
Aug 17, 2019 3:48 PM UTC