You should be able to open, or clone, the project examples under the CubeF1 trees, it might want to pull the STM32F1 pack
Look at construction and meta-data settings of an example
\STM32Cube_FW_F1_V1.8.4\Projects\STM32F103RB-Nucleo\Examples\CRC\CRC_Example\MDK-ARM\Project.uvprojx
To add to something else?
You'd need to set up Include Paths, based on YOUR relativity to them
../Inc;../../../../../../Drivers/CMSIS/Device/ST/STM32F1xx/Include;../../../../../../Drivers/STM32F1xx_HAL_Driver/Inc;../../../../../../Drivers/BSP/STM32F1xx_Nucleo
Add some command line defines for Library and CPU (USE_HAL_DRIVER,STM32F103xB,USE_STM32F1xx_NUCLEO)
Pull in the Library source files to a sub-group in your project
Create a stm32f1xx_hal_conf.h to pull in/enable sub components
STM32Cube_FW_F1_V1.8.4\Projects\STM32F103RB-Nucleo\Examples\CRC\CRC_Example\Inc\stm32f1xx_hal_conf.h
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..