Skip to main content
GRoss.5
Associate II
Jul 30, 2020 3:14 AM UTC
Question

How do I use the IAR I-Jet with the Nucleo-H743ZI2?

  1. I have removed STLINK jumper from JP2.
  2. I have connected I-Jet to MIPI10.
  3. On I-Jet, I see USB and TPWR LEDs are green, and DBG LED is off.
  4. When downloading code get error: CPU did not power up.
  5. None of the Nucleo's LEDs are on. Seems like there is no power to the CPU? I thought the power came from the I-Jet?
This topic has been closed for replies.

3 replies

Imen Ezzine
ST Employee
Jul 30, 2020 2:58 PM UTC

Hi GRoss.5,

To explain this to you, for the Nucleo board there is the possibility to power it using the Stlink, but it is not possible to power it with the I-Jet.

This explains why you receive an error accessing the CPU.

You will need the use of external power (e.g GBF ) in order to power on your Nucleo board.

-Imen

GRoss.5
GRoss.5Author
Associate II
Aug 6, 2020 12:00 AM UTC

Thanks Imen,

I've got the I-jet connected as follows: I-Jet to MIPI10; JP2 set to CHGR; user USB connected to PC; STLINK USB connected to PC. The power is coming from the STLINK USB connection. Is there anyway I can get the power from the user USB connection? This would allow me to remove the connection from STLINK USB to PC.

Tesla DeLorean
Guru
Aug 6, 2020 2:50 AM UTC

>> Is there anyway I can get the power from the user USB connection?

Wire the hot side of R60 or R62 to the 5V side of JP2

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..