Skip to main content
Преслав Колев
Visitor II
Jan 27, 2023 9:06 PM UTC
Question

How can I fix ,,Searching for COM5...Can't open COM5, failed uploading: exit status 1.

Hi everyone,

I have an STM32F103C8 and I want to programm it form Arduino IDE app.The board is booted and all neded addons are already installed from the board manager. Although when I upload the code the app gives this error:

0693W00000Y9N4KQAV.pngI've also tried with the USB to TTL device, but it's the same result. Is there any way to fix that problem?

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jan 30, 2023 1:35 PM UTC

Hello @Пре�?лав Колев and welcome to the Community :)

You have to check your connections, and make sure the cable and board are properly connected.

Check that you've selected the right board in Tools > Board and you've selected the right port in Tools > Port.

Try a different USB cable, different board to make sure that you are using the working one.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks