Skip to main content
Acosi.1
Associate II
Dec 1, 2020 6:45 AM UTC
Question

hi guys i have stm32 nucleo 64 stm32f401 development board i managed to use cubemx and keil to generate a blinking led program which flashed perfectly

but i wanted to try a diffrent ide which was eclipse so i setup the gnu toolchain and tried to flash my led program using stm32 cube programmer but it i did not know what i was doing but i attempted to do a full erase in stm32cube programmer but it only got part way and then gave me an error and i was wondering would stop it from being able to be flashed as i tried it in keil and Iar both gave me errors

Tue Dec 01, 2020 15:39:27: IAR Embedded Workbench 8.40.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\bin\armproc.dll) 

Tue Dec 01, 2020 15:39:27: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\config\debugger\ST\STM32F4xx.dmac 

Tue Dec 01, 2020 15:39:27: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\config\flashloader\ST\FlashSTM32F4xxx.mac 

Tue Dec 01, 2020 15:39:29: Connected to ST-Link/V2-1 [SWD mode 1800 kHz] [Access port: 0] Firmware V2.J37.S26 (Probe no: 57164725) 

Tue Dec 01, 2020 15:39:29: Initial reset was performed 

Tue Dec 01, 2020 15:39:29: 992 bytes downloaded and verified (20.61 Kbytes/sec) 

Tue Dec 01, 2020 15:39:29: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\config\flashloader\ST\FlashSTM32F4xxxRAM96K.out 

Tue Dec 01, 2020 15:39:29: Target reset 

Tue Dec 01, 2020 15:39:29: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\config\flashloader\ST\FlashSTM32F4xxx.mac 

Tue Dec 01, 2020 15:39:29: The flash loader program reported an error. 

Tue Dec 01, 2020 15:39:37: IAR Embedded Workbench 8.40.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\bin\armproc.dll) 

and keil gave similar error is it possible erasing it could be the problem

This topic has been closed for replies.