Skip to main content
islavv
Associate III
Oct 14, 2025 11:39 AM UTC
Question

Has anyone else struggled with the MX3080/M1400 Wi‑Fi modules?

Honestly, this choice feels like a trap.

STM keeps promoting it as a “solution,” but compared to Murata, ESP32, or Broadcom it looks outdated:

– Legacy M4 core, original MXCHIP code from 2017

– Closed software, very little documentation

– Hard to debug (no sequence diagrams, no clear dedicated examples)

– Rare, unpolished firmware updates

– No Nucleo board for hands‑on exploration

– Doesn’t seem seriously supported by MXCHIP anymore (similar by STM)

This isn’t a shallow impression — I spent three weeks with console access and a logic analyzer writing and debugging code on the B‑U585I‑IOT2A board, and the friction was constant.

Curious if others see the same issues, or if there’s a hidden advantage I’m missing?

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Oct 14, 2025 11:42 AM UTC

Prompted by this ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
islavv
islavvAuthor
Associate III
Oct 14, 2025 1:07 PM UTC

I was eventually able to get the MX3080 Wi‑Fi running properly, but only after working through a number of issues that really should have been better explained and documented by ST and not explored with logical analyzer and soldering console port to chip. From what I’ve seen, ST’s policy is to take no responsibility for non‑ST parts, even when they’re included on ST demo boards, and MXCHIP itself doesn’t appear to be very actively maintained anymore.

Because I had to dig into clock settings, pin modes, SPI, and interrupt configurations step by step, I can appreciate how challenging this path could be for others approaching it for the first time.

Andrew Neil
Super User
Oct 14, 2025 1:40 PM UTC

@islavv wrote:

From what I’ve seen, ST’s policy is to take no responsibility for non‑ST parts, even when they’re included on ST demo boards


Even when they're promoted as "Partners":

https://community.st.com/t5/stm32-mcus-products/new-madeforstm32-what-does-it-actually-mean/m-p/131466

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.