Skip to main content
Kleber Lima da Silva
Associate
Jan 10, 2017 2:27 PM UTC
Solved

Hard fault to read internal EEPROM - STM32L011

Posted on January 10, 2017 at 15:27

Hi,

I am getting a hard fault while trying to read from the internal EEPROM (STM32L011), function:

uint8_t Read_EEPROM_Byte(uint32_t address)

{

   uint8_t tmp = 0;

   address = address + 0x08080000;

   tmp = *(uint32_t*)address;

   return tmp;

}

How to solve this?

Thanks.

#stm32l0 #eeprom
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 10, 2017 4:24 PM UTC
Posted on January 10, 2017 at 17:24

Pro tip: When debugging Hard Faults, Look at the address it is complaining about, print it out, or look at it in the debugger.

The Cortex-M0 does not support unaligned read/write operations, and will also fault if you touch memory out of bounds. Use appropriate casting.

uint8_t Read_EEPROM_Byte(uint32_t address)
{
 uint8_t tmp = 0;
 address = address + 0x08080000;
 tmp = *(uint8_t*)address; // READ AS A BYTE
 return tmp;
}

uint8_t Read_EEPROM_Byte(uint32_t address)
{
 return(*(uint8_t*)(address + 0x08080000));
}�?�?�?�?�?�?�?�?�?�?�?�?�?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

6 replies

Jeroen3
Senior
Jan 10, 2017 3:29 PM UTC
Posted on January 10, 2017 at 16:29

You're most likely performing a unaligned memory access.

 tmp = *(uint32_t*)address;

You are now trying to read 4 bytes from address into tmp. (of which the 3 most significant bytes will be truncated)

However, if address is uneven, eg:

0x*1, it's an illegal operation.

Remember, you can only access words on a word aligned address.

0x08080000

halfword / word aligned

0x08080002 halfword aligned

0x08080004 word aligned

...

Byte reads are always allowed by the core.

Some peripherals also limit the types of read/write to their memory region. 

This doesn't apply to reading here. It does to writing.

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 10, 2017 4:24 PM UTC
Posted on January 10, 2017 at 17:24

Pro tip: When debugging Hard Faults, Look at the address it is complaining about, print it out, or look at it in the debugger.

The Cortex-M0 does not support unaligned read/write operations, and will also fault if you touch memory out of bounds. Use appropriate casting.

uint8_t Read_EEPROM_Byte(uint32_t address)
{
 uint8_t tmp = 0;
 address = address + 0x08080000;
 tmp = *(uint8_t*)address; // READ AS A BYTE
 return tmp;
}

uint8_t Read_EEPROM_Byte(uint32_t address)
{
 return(*(uint8_t*)(address + 0x08080000));
}�?�?�?�?�?�?�?�?�?�?�?�?�?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Shay Eliyahu
Visitor II
Dec 11, 2017 11:08 AM UTC
Posted on December 11, 2017 at 11:08

Hello Clive One,

what about to Unlock the EEPROM and lock it back??

Tesla DeLorean
Guru
Dec 11, 2017 3:34 PM UTC
Posted on December 11, 2017 at 15:34

This post is from 11 months ago, a lot of the surrounding code is not shown, the cause of the fault in this case was the unaligned access. At the top level you might well need to lock/unlock the EEPROM, I'm sure the library has worked examples.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Kleber Lima da Silva
Associate
Jan 10, 2017 4:36 PM UTC
Posted on January 10, 2017 at 17:36

Thanks Jeroen3 and Clive One.

Solved!

Shay Eliyahu
Visitor II
Dec 11, 2017 11:09 AM UTC
Posted on December 11, 2017 at 11:09

Hello Kleber,

what about to Unlock the EEPROM and lock it back??