Skip to main content
xrstokes
Associate III
Dec 18, 2018 6:46 AM UTC
Question

HAL_SPI_Receive() Pins not doing anything.

Hi, I'm new to this environment. I try never to ask questions on forums but I've been stuck for over a week. I set up a blue pill board and tried a simple SPI setup of a single 74HC595 and a single 74HC165. I got the 595 working great with this code.

	message = 8;
 
	HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, false);
	HAL_Delay(100);
	HAL_SPI_Transmit(&hspi1, (uint8_t *)message, 1, HAL_MAX_DELAY);
	HAL_Delay(100);
	HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, true);
	HAL_Delay(1000);

This can be used to switch any of the pins on the 595. I assumed the following code would read the input.

uint8_t receive;
 
	while(true)
	{
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, false);
	HAL_Delay(100);
	HAL_SPI_Receive(&hspi1, receive, 1, HAL_MAX_DELAY);
	HAL_Delay(100);
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, true);
	HAL_Delay(1000);
 
	Debug_Print(receive);
	}

But no luck. If i scope the the sclk pin it doesn't even send the clock pulses. another interesting thing is that if i include this receive code and the transmit code. the transmit code stops working?

here is my SPI setup

static void MX_SPI1_Init(void)
{
 __HAL_RCC_SPI1_CLK_ENABLE();
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 10;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
}

Thanks in advance, I don't have a forum home for this ide yet. This is me looking for one.

This topic has been closed for replies.