Skip to main content
Associate II
Apr 28, 2026 10:03 AM UTC
Question

Going back to older version of code

Hey guys!

I am currently working with Secure Boot using ARM TrustZones, Secure and Non-Secure!

I have ***ed up my code majorly hehe, and I cant just Ctrl + Z everything since I have edited in a lot of files and generated code from CubeMX (UART, HAL, HASH etc), is there a smooth way to go back to an older version of the entire folder, for example an older version of NonSecure and Secure etc.

Thanks in advance!

4 replies

Andrew Neil
Super User
Apr 28, 2026 10:11 AM UTC

Do you use a version control system (VCS); eg, Git ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Apr 28, 2026 10:41 AM UTC

No, unfortunatley not, I am only using STM32CubeIDE, which is why I came here to ask!

Andrew Neil
Super User
Apr 28, 2026 10:48 AM UTC

In that case, no.

This is exactly why Software Version Control Systems (SVCS) exist - so now would be the time to start using one!

Git is probably the most widely used nowadays, although others are available.

GitHub, as the name suggests, uses Git and also provides a hosting service.

GitLab is another, and there are many, many more.

 

PS:

You can host Git locally, but that's a load of extra work and loses the benefit of having an off-site backup.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.