Associate
April 25, 2013
Question
Getting Speaker Tone from DAC Peripheral
- 3 replies
- 1667 views
Posted on April 25, 2013 at 20:46
Hello,
I am a first time poster on this forum so please bear with me. I am using CMSIS to get the DAC peripheral to play a simple tune. I am working off an example I found online which I have simplified to play only one note (single tone) before moving on to the tune. I am able to build the target, however, when I download it onto the micro-controller, nothing happens. It was suggested to me that this may be due to my not having set a frequency to the DAC, specifically one that would be audible to the human ear. If this is the case, I am curious why this was not touched upon in the example provided and why it is not mentioned in the DAC peripheral files (.c, .h) in CMSIS? Furthermore, I was under the impression that the timer trigger that I've used (see attached) would dictate the frequency of the tone. Is this not the case? If the issue I am having is not related to frequency, I would appreciate any advice that could point me in the right direction. I've included a zip of the working example I found online as well as the main.c file of the code I used to implement my design. The rest is just standard CMSIS that I found on the site. Any help would be greatly appreciated. Thanks in advance, Yusif Nurizade #stm32f4discovery-dac-audio #cmsis-keil-peripheral-library