Skip to main content
JStrz.1
Associate
Nov 25, 2020 9:52 AM UTC
Question

FLASH memory reservation for settings storage.

Hi

Maybe similar topic has already been there, but I can't find it...

I am using CubeMX and HAL on the 446RE.

I can write and read data to / from FLASH (In this case directly, I do not use EEPROM emulation).

Question: Where and how to set, e.g. Sector3 that it was only for my data. So that it is not overwritten during programming etc. I understand it like this: The program code is e.g. in sectors 0,1,2,4 and 5. The compiler prepares the batch in such a way that it skips sector 3.

Can it be set in the program code or somewhere in the CubeMX settings?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Nov 25, 2020 12:12 PM UTC

With GNU based tools you'd typically change the linker script (.ld) to describe two sections of memory, and then direct content into them.

​

The linker isn't that smart, and you might want to automate the generation of a working set​ of functions or objects

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..