Skip to main content
Evgeny Erlihman
Associate III
Oct 30, 2017 6:18 PM UTC
Solved

External JLink with Nucleo 144

Posted on October 30, 2017 at 19:18

Hello,

I am trying to use my JLink Ultra+ with stm32h7 nucleu 144 board. I followed the instructions on:

https://gnu-mcu-eclipse.github.io/developer/j-link-stm32-boards/

 

but could not make it work, after connecting all the pins, i removed the CN4 jumpers. At this point i see that the probe senses the board, but the sw4stm still gives me an error about unconnected board....

Has anybody been able to use an external JLink probe with a nucleu 144 board?

I am using sw4stm IDE.

Thanks,

Evgeny

#sw4stm32-eclipse #stm32h7 #segger #jlink #sw4stm32
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Oct 31, 2017 4:33 PM UTC
Posted on October 31, 2017 at 16:33

I would connect to the target using the CN4 SWDIO/SWCLK pins, currently you are talking back into the ST-LINK, not the target

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

8 replies

Tesla DeLorean
Guru
Oct 30, 2017 8:21 PM UTC
Posted on October 30, 2017 at 21:21

Use the JLink Commander tools to check connectivity/function.

Watch the NRST and SWO connectivity, and remove solder-bridges connecting to the on-board ST-LINK

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Evgeny Erlihman
Associate III
Oct 30, 2017 9:37 PM UTC
Posted on October 30, 2017 at 21:37

Just to make sure i understood you, the solder bridges need to be removed are SB110 (SWO) & SB111 (NRST)?

Tesla DeLorean
Guru
Oct 31, 2017 12:16 AM UTC
Posted on October 31, 2017 at 00:16

Yes, the schematic should be illustrative of this also.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..