Skip to main content
YFuku.3
Associate III
Jan 20, 2019 6:25 AM UTC
Solved

Error: selected processor does not support `dsb 0xF' in Thumb mode

board: NucleoG071RB

An error happens when I compile codes. There is no error like this when I compile codes in STM32L053

Building file: ../Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_cortex.c

Invoking: MCU GCC Compiler

/Users/username/Documents/stm32cubemx/test/Debug

arm-none-eabi-gcc -mthumb -mfloat-abi=soft '-D__weak=__attribute__((weak))' '-D__packed="__attribute__((__packed__))"' -DUSE_HAL_DRIVER -DSTM32G071xx -I"/Users/username/Documents/stm32cubemx/test/Inc" -I"/Users/username/Documents/stm32cubemx/test/Drivers/STM32G0xx_HAL_Driver/Inc" -I"/Users/username/Documents/stm32cubemx/test/Drivers/STM32G0xx_HAL_Driver/Inc/Legacy" -I"/Users/username/Documents/stm32cubemx/test/Drivers/CMSIS/Device/ST/STM32G0xx/Include" -I"/Users/username/Documents/stm32cubemx/test/Drivers/CMSIS/Include" -Og -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF"Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_cortex.d" -MT"Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_cortex.o" -o "Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_cortex.o" "../Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_cortex.c"

/var/folders/gs/z19g5t5131bcqw3kq_h9knkw0000gn/T//ccU0K4oV.s: Assembler messages:

/var/folders/gs/z19g5t5131bcqw3kq_h9knkw0000gn/T//ccU0K4oV.s:234: Error: selected processor does not support `dsb 0xF' in Thumb mode

/var/folders/gs/z19g5t5131bcqw3kq_h9knkw0000gn/T//ccU0K4oV.s:249: Error: selected processor does not support `dsb 0xF' in Thumb mode

/var/folders/gs/z19g5t5131bcqw3kq_h9knkw0000gn/T//ccU0K4oV.s:696: Error: selected processor does not support `dsb 0xF' in Thumb mode

/var/folders/gs/z19g5t5131bcqw3kq_h9knkw0000gn/T//ccU0K4oV.s:707: Error: selected processor does not support `isb 0xF' in Thumb mode

/var/folders/gs/z19g5t5131bcqw3kq_h9knkw0000gn/T//ccU0K4oV.s:744: Error: selected processor does not support `dmb 0xF' in Thumb mode

make: *** [Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_cortex.o] Error 1

Please advise me

This topic has been closed for replies.
YFuku.3
YFuku.3Best answer
Associate III
Jan 20, 2019 4:31 PM UTC

I updated sw4stm32 and then work out!

4 replies

turboscrew
Senior III
Jan 20, 2019 9:18 AM UTC

My guess is that there's some mix-up of architectures. Different architectures can have different points of coherence parameter to DSB. I'm not sure, but maybe the points of coherence are differently coded. Usually the point of coherence used is SYSTEM (DSB SY). I recall (vaguely), however that SY is usually coded as 0xF. The ARM ARM (Architecture Reference Manual) for your core shows what points of coherence the architecture supports and how they are coded. STM32F071RB is Cortex M0 device, and the manual is ARMv6-M ARM. STM32L053 is Cortex M0+ device, but the architecture is still the same ARMv6.

turboscrew
Senior III
Jan 20, 2019 9:19 AM UTC

Another thing could be the C compiler.

YFuku.3
YFuku.3AuthorBest answer
Associate III
Jan 20, 2019 4:31 PM UTC

I updated sw4stm32 and then work out!

AKarg.14
Visitor II
Sep 30, 2019 12:54 PM UTC

How did you update sw4stm32 ?