Skip to main content
YFuku.3
Associate III
Jan 20, 2019 4:49 PM UTC
Question

Error "OpenOCD child process termination" happens

environment: Nucleo-G071RB, sw4stm32

when I click "Run", the following dialog shows up

-------------------

Error "OpenOCD child process termination" happens

Reason: wrong device detected, check the board connected.

-------------------

console is here

-------------------

Open On-Chip Debugger 0.10.0-dev-00015-gaaf1808 (2018-11-13-12:57)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 240 kHz

adapter_nsrst_delay: 100

Info : clock speed 240 kHz

Info : STLINK v2.1 JTAG v31 API v2 M21 VID 0x0483 PID 0x374B

Info : using stlink api v2

Info : Target voltage: 3.247800

Info : Stlink adapter speed set to 240 kHz

Info : STM32L053R8Tx.cpu: hardware has 4 breakpoints, 2 watchpoints

Info : Stlink adapter speed set to 240 kHz

adapter speed: 240 kHz

target halted due to debug-request, current mode: Thread 

xPSR: 0xf1000000 pc: 0x08003bf8 msp: 0x20000890

STM32L0: Enabling HSI16

Info : Stlink adapter speed set to 4000 kHz

adapter speed: 4000 kHz

** Programming Started **

auto erase enabled

Warn : Cannot identify target as a STM32L family.

Error: auto_probe failed

** Programming Failed **

shutdown command invoked

-------------------

it is confusing that even though I use STMG071RB, the OpenOCD targets STM32L family. Please advise.

Thanks!

This topic has been closed for replies.

1 reply

Andreas Bolsch
Lead III
Jan 20, 2019 7:33 PM UTC