Skip to main content
mafix mafix
Associate II
September 3, 2017
Solved

EEPROM Problem

Posted on September 03, 2017 at 14:38

Hello,

I use HAl_Flash driver on STM32L152RBT6 to read, write and erase internal flash memory(EEPROM).

when i try to write new data to flash, thatbitwise OR with previous value.

(

E.g. at address 0x08007000 pre-save =(int) 5, data =(int) 16 stored-value = (int) 21)

so i need to erase at the specified address before try to store new data on it.

In datasheet clearly explained how can erase

a word (unsigned int ** 4Byte).

Data EEPROM word erase

This operation is used to erase a word in Data EEPROM. To do so:

  • Unlock the Data EEPROM and the FLASH_PECR register
  • Write a word to a valid address in data EEPROM with the value 0x0000 0000
  • This activates an erase phase

code:

uint32_t Address = 0x08007900;
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
*(uint32_t *)Address = (uint32_t) 0x00;
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
�?�?�?�?�?�?

but it doesn't work.

if i set ERASE and PROG bits whole the page(256Byte) will be erased!

SET_BIT(FLASH->PECR, FLASH_PECR_ERASE);
SET_BIT(FLASH->PECR, FLASH_PECR_PROG);�?�?

what can i do for erasing 1 byte or 1 word?

thanks.

#eeprom #flash-erase
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 3, 2017
Posted on September 03, 2017 at 18:30

Perhaps you should be using the EEPROM, which is situated at 0x08080000..0x08080FFF ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Guru
September 3, 2017
Posted on September 03, 2017 at 16:19

HAL_FLASHEx_DATAEEPROM_Unlock()

HAL_FLASHEx_DATAEEPROM_Erase(FLASH_TYPEERASEDATA_WORD,0x08007900);

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mafix mafix
Associate II
September 3, 2017
Posted on September 03, 2017 at 17:02

Thanks to reply.

Also HAL_FLASHEx_DATAEEPROM_Erase() not erase anything. Just can erase full page but not a word or a byte.

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 3, 2017
Posted on September 03, 2017 at 18:30

Perhaps you should be using the EEPROM, which is situated at 0x08080000..0x08080FFF ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..