Skip to main content
sarojj7
Associate II
May 22, 2020 2:09 PM UTC
Question

EEPROM Emulation without using HAL

Dear All,

Board: Nucleo - H745ZI-Q

I want to store few bytes of non volatile memory, for which I learnt that I need to use EEPROM emulation code. I went through the code given as part of STM software in en.stm32cubeh7_v1-7-0\STM32Cube_FW_H7_V1.7.0\Projects\NUCLEO-H7A3ZI-Q\Applications\EEPROM\EEPROM_Emulation\MDK-ARM . I find that there are several HAL calls made in the code.

What I require is, to have a code without HAL calls that is in terms of low level drivers or register read/write. Till now I managed to not use HAL, would like to continue this way. Kindly help.

This topic has been closed for replies.