ebyte e220 LoRa receiving problem
- 1 reply
- 446 views
Hello,
I’m working on a LoRa(e220-400t22d) communication project using an F411 Blackpill and a Nucleo F446 board. The Blackpill is connected to the transmitter LoRa module, while the Nucleo board is connected to the receiver module.
On the transmitter side, I’m reading a 12-bit ADC value and packaging it for transmission. Using the debugger, I can correctly monitor the variables on the transmitter. However, after flashing the code and powering up the transmitter, when I debug the receiver board, I can’t see any variable values updating at all.
Note: I’ve configured both LoRa modules to have the same address and channel(etc.) settings. While the transmitter LoRa module warms up, there is no activity on the receiver LoRa side. I’ve attached both transmitter and receiver main.c files for reference.