Skip to main content
Edward Jang
Associate
Dec 21, 2018 2:13 AM UTC
Question

Doesn't IAR Compiler support STM32L496ZGTxP?

I use Iar Embedded Workbench 8.32.2.194323.

I created the project file with Cubemx 5.0 using STM32L496ZGTxP.(Nucleo-L496ZG-P).

I didn't nothing in the cubemx 5.0.

It works well in STM32L496ZGTx. (Nucleo-L496ZG).

When I compiled In the IAR workbench, Iar workbench shows these error messages.

=============================

Building configuration: STM32L496ZGTxP2 - STM32L496ZGTxP2 

Updating build tree... 

startup_stm32l496xx.s 

Error[438]: This instruction is not available in the selected cpu/core F:\Work\STM32L496ZGTxP2\EWARM\startup_stm32l496xx.s 189 

Error while running Assembler 

stm32l4xx_hal_dma.c  

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1792 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1797 

Error while running C/C++ Compiler 

stm32l4xx_hal.c  

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1792 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1797 

Error while running C/C++ Compiler 

main.c  

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1792 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1797 

Error while running C/C++ Compiler 

stm32l4xx_hal_cortex.c  

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1792 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\CMSIS\Include\core_cm4.h 1797 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DMB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\STM32L4xx_HAL_Driver\Src\stm32l4xx_hal_cortex.c 443 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_DSB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\STM32L4xx_HAL_Driver\Src\stm32l4xx_hal_cortex.c 472 

Error[Ta148]: Intrinsic function "__nounwind __iar_builtin_ISB" is not available in this architecture F:\Work\STM32L496ZGTxP2\Drivers\STM32L4xx_HAL_Driver\Src\stm32l4xx_hal_cortex.c 473 

This topic has been closed for replies.

2 replies

ST Technical Moderator
Dec 26, 2018 1:28 PM UTC

Hello @Edward Jang​ ,

I think the "Use CMSIS" option is not checked. Thus the CMSIS intrinsic are not found.

You can set the CMSIS-DSP library option in the Project > Options, then General Options>Library Configuration page.

If your issue is not resolved, could you please share the ioc file to check that may be an issue related to CubeMX project generation.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
NM.1
Associate II
Jan 7, 2020 9:10 AM UTC

Hi @Edward Jang​ ,

I also faced similar problem but for another controller.

The problem was with wrong setting of core. It worked after selecting proper controller.

This you can find under Project ->Options->General Options->Target

You can check what core(in your case it will be Cortex-M4 core) or device selected(STM32L496ZG).