Skip to main content
roboSaga
Associate
Apr 1, 2019 8:21 AM UTC
Question

Debugger *.elf file erase the data.

I use NUCLEO-H743ZI with TrueSTUDIO.

I write some datas to flash memory 0x081e 0000 (bank=2,sector=7).

This address is separate from the program downloaded,

but when I start Debugger, *.elf file erase the data.

What's the problem?

I confirmed the data is correctly written on memory using ST-LINK utility.

This topic has been closed for replies.

6 replies

AvaTar
Senior III
Apr 1, 2019 9:04 AM UTC

> ... *.elf file erase the data

No, ELF files don't erase data. The debugger does.

I'm not familiar with TrueStudio, but doing a mass-erase before flashing is a IDE/debugger setting.

All modern toolchains I'm familiar with have an option to update only modified sectors.

roboSaga
roboSagaAuthor
Associate
Apr 1, 2019 9:27 AM UTC

Thank you for the your advice.

I will check the tool settings a little more.

Pavel A.
Apr 1, 2019 1:50 PM UTC

In Eclipse this option is in the debug configuration:

roboSaga
roboSagaAuthor
Associate
Apr 3, 2019 12:36 AM UTC

Thank you for your polite advice.

I noticed another problem.

When I write code to operate flash memory, the data written to flash memory

does not disappear. for example, HAL_FLASH_Unlock() etc.

Even before the code is actually executed.

However, if I delete this code (HAL_FLASH_Unlock() etc.), and launch the debugger,

the data written to flash memory will disappear.

I may have missed something or misunderstood it.

I will try hard more.

Thank you very much.

Tesla DeLorean
Guru
Apr 3, 2019 2:17 AM UTC

With the level of information it is going to be very hard to guess what you're really doing and why it is failing.

Cherry picking one line of code with HAL_FLASH_Unlock() provides no context to the larger issues and interactions.

Perhaps dump the ELF object and see if it touches any of the regions involved.

Instrument your code so you can see what it is doing, and put bounds checking around any write or erase functions so it prevents you from touching the memory blocks the code is executing from.

Perhaps create a simple/minimal project that demonstrates your issue, and zip up the project including the output files, and attach the .ZIP here.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
roboSaga
roboSagaAuthor
Associate
Apr 3, 2019 9:41 AM UTC

Thank you for your kind suggestion.

I found a new condition.

If I write a *.hex file by STLink tool one time I can debug with TrueStudio.

The data written to the flash memory remains .

I will try by myself a little more.

Thank you