Skip to main content
Associate II
Jul 11, 2026 9:26 AM UTC
Question

Communication of LAN9253 with STM32F446ZCH6 using Quad SPI

I am trying to establish communication between an STM32F446ZCH6 and a LAN9253 using the Quad SPI (QSPI) interface on our custom hardware.

As an initial validation, I am attempting to read the following LAN9253 registers:

  • BYTE_TEST register (0x64)

  • ID_REV (Chip ID) register (0x50)

However, I am not receive the expected register values. Instead, the values returned are consistently 0x88888888 or 0xFFFFFFFF.

To troubleshoot the issue, I captured the SPI/QSPI communication using a logic analyzer. From the waveforms, it appears that:

  • The STM32 (master) is transmitting the read command correctly.

  • The clock (SCK) and chip select (CS) signals appear normal.

  • However, the LAN9253 does not respond with valid data, and the STM32 does not receive any meaningful data from the slave.

We also attempted communication using:

  • Single SPI (1-bit mode)

  • Dual SPI (2-bit mode)

  • Quad SPI (4-bit mode)

Unfortunately, the behavior is the same in all three modes, with no valid response from the LAN9253.

We have verified the hardware and found the following:

  • LAN9253 supply voltage: 3.3 V (stable)

  • RESET pin: High (device is out of reset)

  • Crystal oscillator: 25 MHz, confirmed on the oscilloscope

One additional observation from the logic analyzer is that:

  • IO3 remains pulled high throughout the communication.

  • IO0, IO1, and IO2 remain low, and no response is observed from the slave device.

This is a custom board containing the STM32F446ZCH6 and LAN9253.

I will attach:

  • Logic analyzer waveform screenshots

  • Relevant source code used for the register read operation

Has anyone encountered a similar issue with the LAN9253? Are there any additional hardware checks, initialization steps, bootstrap requirements, or QSPI/SPI timing considerations that I should verify? Any suggestions would be greatly appreciated.

1 reply

waclawek.jan
Super User
Jul 13, 2026 11:54 AM UTC

I don’t use the chip you mention and I don’t know answers to your questions, but you may want to start with bit-banging the protocol first.

JW