Skip to main content
Senior
Jun 2, 2025 12:32 PM UTC
Solved

Clock issues in STM32H753ZI100_24 - SystemClock_Config() hangs

I have been using the STM32H753ZI100_24  for getting pressure data from the MS5611-01BA03 mems sensor. The debugger stops at SystemClock_Config() function in the code of reading prom registers from the MS5611-01BA03  sensor as per the datasheet Barometre datasheet 

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MPU Configuration--------------------------------------------------------*/
 MPU_Config();

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI1_Init();
 /* USER CODE BEGIN 2 */
 uint16_t prom[8] = {0};

 uint8_t rst_cmd = 0x1E; // Reset command
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
 HAL_SPI_Transmit(&hspi1, &rst_cmd, 1, HAL_MAX_DELAY);
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
 HAL_Delay(3);



// if (MS5611_ReadPROM(prom) == HAL_OK) {
// // Now prom[] contains all PROM coefficients including factory data and CRC
// for (int i = 0; i < 8; i++) {
//	 printf("PROM[%d] = %u\n", i, prom[i]);
// }
// } else {
// printf("Error reading PROM!\n");
// }

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 MS5611_ReadPROM(prom);
	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */
}

I will also attach the SystemClock_Config function.

 
void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};


/** Supply configuration update enable

 */

 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);


/** Configure the main internal regulator output voltage

 */

 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);


while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}


/** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM = 25;

 RCC_OscInitStruct.PLL.PLLN = 200;

 RCC_OscInitStruct.PLL.PLLP = 20;

 RCC_OscInitStruct.PLL.PLLQ = 20;

 RCC_OscInitStruct.PLL.PLLR = 2;

 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_0;

 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;

 RCC_OscInitStruct.PLL.PLLFRACN = 0;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

 Error_Handler();

 }


/** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2

 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;

 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;

 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;


if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

 {

 Error_Handler();

 }

}

Here the debugger stops at the Error_Handler() function of the statement

 
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

 Error_Handler();

 }

So I step into HAL_RCC_OscConfig() function where it shows

_weak HAL_StatusTypeDef HAL_RCC_OscConfig(RCC_OscInitTypeDef *RCC_OscInitStruct)
{
 uint32_t tickstart;
 uint32_t temp1_pllckcfg, temp2_pllckcfg;

 /* Check Null pointer */
 if (RCC_OscInitStruct == NULL)
 {
 return HAL_ERROR;
 }

 /* Check the parameters */
 assert_param(IS_RCC_OSCILLATORTYPE(RCC_OscInitStruct->OscillatorType));
 /*------------------------------- HSE Configuration ------------------------*/
 if (((RCC_OscInitStruct->OscillatorType) & RCC_OSCILLATORTYPE_HSE) == RCC_OSCILLATORTYPE_HSE)
 {
 /* Check the parameters */
 assert_param(IS_RCC_HSE(RCC_OscInitStruct->HSEState));

 const uint32_t temp_sysclksrc=__HAL_RCC_GET_SYSCLK_SOURCE();
 const uint32_t temp_pllckselr = RCC->PLLCKSELR;
 /* When the HSE is used as system clock or clock source for PLL in these cases HSE will not disabled */
 if ((temp_sysclksrc== RCC_CFGR_SWS_HSE) || ((temp_sysclksrc== RCC_CFGR_SWS_PLL1) && ((temp_pllckselr & RCC_PLLCKSELR_PLLSRC) == RCC_PLLCKSELR_PLLSRC_HSE)))
 {
 if ((__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) != 0U) && (RCC_OscInitStruct->HSEState == RCC_HSE_OFF))
 {
 return HAL_ERROR;
 }
 }
 else
 {
 /* Set the new HSE configuration ---------------------------------------*/
 __HAL_RCC_HSE_CONFIG(RCC_OscInitStruct->HSEState);

 /* Check the HSE State */
 if (RCC_OscInitStruct->HSEState != RCC_HSE_OFF)
 {
 /* Get Start Tick*/
 tickstart = HAL_GetTick();

 /* Wait till HSE is ready */
 while (__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) == 0U)
 {
 if ((uint32_t)(HAL_GetTick() - tickstart) > HSE_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }
 }
 else
 {
 /* Get Start Tick*/
 tickstart = HAL_GetTick();

 /* Wait till HSE is disabled */
 while (__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) != 0U)
 {
 if ((uint32_t)(HAL_GetTick() - tickstart) > HSE_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }
 }
 }
 }

In this function since i have only enable HSE clock but our custom board have both HSE and LSE in it.

Coming back to code in this HAL_RCC_OscConfig() function the debugger stops at the below while loop

while (__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) == 0U)
 {
 if ((uint32_t)(HAL_GetTick() - tickstart) > HSE_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }

it toggles between while() statement and if() statement. is it normal for the oscillator to start after toggling it so many times or is the there any problem in enabling clock from my side
the clock for spi is connected to APB2 which is 25 MHz. I have attach the photo of the clock configuration of the above project.
Screenshot from 2025-06-02 18-09-03.png

 

and the stm32 datasheet stm32 datasheet which we are using.

This topic has been closed for replies.
TDK
TDKBest answer
Jun 2, 2025 12:47 PM UTC

If HSERDY fails to get set, there is probably an issue with the HSE oscillator circuit. Can you show your schematic? Ensure the oscillator and load caps are appropriate.

"If you feel a post has answered your question, please click ""Accept as Solution""."

23 replies

TDK
TDKBest answer
Jun 2, 2025 12:47 PM UTC

If HSERDY fails to get set, there is probably an issue with the HSE oscillator circuit. Can you show your schematic? Ensure the oscillator and load caps are appropriate.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Senior
Jun 2, 2025 1:52 PM UTC

yes i checked with the team. its due to the problem with the oscillator

Andrew Neil
Super User
Jun 2, 2025 1:44 PM UTC

This doesn't seem to have anything at all to do with the MS5611-01BA03 mems sensor - SystemClock_Config() is called long before anything happens related to the sensor!

So it's purely an STM32 thing?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Senior
Jun 2, 2025 2:03 PM UTC

hey andrew, thanks for the reply i check with the team yes its the problem with the oscillator. now, if i get data from the prom register how can i consider it as the correct one. is there is known values given for any registers i can compare the values with that. or possibility of modify the values to get the known values. can i search this in a forum

Andrew Neil
Super User
Jun 2, 2025 2:18 PM UTC

@santhosh16 wrote:

hey andrew, thanks for the reply i check with the team yes its the problem with the oscillator. 


OK - I'll edit the title to clarify.

 


@santhosh16 wrote:

 now, if i get data from the prom register how can i ...


That's an entirely different question!

You won't be able to do anything at all until you have fixed the clock problem.

 

For how to communicate with the MS5611-01BA03 mems sensor, and interpret the data from it, you will have to study the manufacturer's datasheet & any other supporting information.

The MS5611-01BA03 is a TE product - nothing to do with ST - so you will need to contact TE for support with it.

 

The recommended approach would be to get a development/evaluation kit from TE, and use an ST board (eg, Nucleo) to get you started with known-good hardware.

 

It seems that 3rd-party breakout boards are also available; eg,

https://www.amazon.co.uk/MS5611-01BA03-Atmospheric-Pressure-Altimeter-Electronic/dp/B07Y1QZKF4

AndrewNeil_1-1748873892831.png

 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Jun 2, 2025 1:59 PM UTC

Hello,


@santhosh16 wrote:

The debugger stops at SystemClock_Config() function in the code of reading prom registers from the MS5611-01BA03  sensor .


Not sure if I understood this statement.

The system clock is a first stage clock initialization of the MCU. The sensor config (I think SPI) comes after.

So if your application presents issue at SystemClock_config() this means you have an issue with the clock config on your MCU. 

As you selected HSE as system clock  source:

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

You need to be sure that your crystal is OK.

You need to post your schematic.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Senior
Jun 2, 2025 2:07 PM UTC

hey mƎALLEm, I have check with the team the external clock is the problem here. now i using the internal clock

Now, if i get data from the prom register how can i consider it as the correct one. is there is known values given for any registers i can compare the values with that. or possibility of modify the values to get the known values. can i search this in a forum

mƎALLEm
ST Technical Moderator
Jun 9, 2025 12:51 PM UTC

@santhosh16 

Please state on this post. Did you solve the issue?

If one of the comments answered your question or at least guided you to the solution, please accept it as solution by clicking the button:

mALLEm_0-1749473450862.png

Thank you for your understanding.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Senior
Jun 9, 2025 12:59 PM UTC

but before i try one of these solutions, i got the error stlink is not initialized  which i queried before in this community. so once after clear that issue i can come into solving this.