Skip to main content
Associate
Aug 22, 2026 5:01 PM UTC
Solved

Can i Use Realtek RTL8211F-CG with Stm32H7

Hi everyone,

I have a schematic using the Realtek RTL8211F-CG Gigabit Ethernet PHY and I want to connect it directly to an STM32H7 microcontroller for Ethernet communication.

My questions are:

  1. The STM32H7 Ethernet MAC supports MII and RMII only. The RTL8211F-CG is a Gigabit PHY that primarily uses RGMII. Is there any way to make it work with STM32H7 without adding an intermediate chip like LAN8720 or DP83848?
  2. The RTL8211F-CG datasheet mentions it can operate at 10/100 Mbps as well but does it support a true RMII mode that the STM32H7 MAC can talk to?
  3. Has anyone successfully used the RTL8211F-CG with STM32H7 directly? If so, what interface mode did you configure on the PHY side, and what changes were needed in CubeMX/HAL?
  4. If this is not possible at all, what is the simplest/cheapest alternative 10/100 PHY that works reliably with STM32H7 in RMII mode?

Any help or experience is appreciated. Thanks!

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Aug 27, 2026 8:43 AM UTC

Hello,

A question that you need to address to Realtek

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

Andrew Neil
Super User
Aug 22, 2026 5:03 PM UTC

@Meer  wrote:

2. The RTL8211F-CG datasheet mentions it can operate at 10/100 Mbps as well but does it support a true RMII mode that the STM32H7 MAC can talk to?


You would have to ask RealTek that.

 


@Meer  wrote:

4. If this is not possible at all, what is the simplest/cheapest alternative 10/100 PHY that works reliably with STM32H7 in RMII mode?


Simplest, surely, would be to use whatever the ST boards use?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MeerAuthor
Associate
Aug 22, 2026 5:07 PM UTC

Thanks for your comment. I will asked to RealTek

Senior III
Aug 22, 2026 5:03 PM UTC

No, you generally cannot connect RTL8211F-CG directly to an STM32H7 Ethernet MAC.

The problem is not the 10/100/1000 capability on the cable side. The issue is the MAC-to-PHY interface. STM32H7 Ethernet supports MII/RMII, while RTL8211F-CG is mainly an RGMII PHY. Even when the RTL8211F-CG negotiates 10 or 100 Mbps on the Ethernet cable, the MAC-side interface is still RGMII, just running at lower clock rates. It does not magically become RMII.

So unless your STM32H7 variant has an RGMII-capable Ethernet MAC, which normal STM32H7 parts do not, CubeMX/HAL cannot fix this in software. The pinout, clocking, and data bus are physically different.

For STM32H7, the simpler solution is to use a 10/100 RMII PHY such as:

  • LAN8720 / LAN8742

  • DP83848

  • KSZ8081 / KSZ8091

  • RTL8201

LAN8742 is commonly used on ST boards, so it is usually the safest choice with CubeMX examples.

In short: RTL8211F-CG is fine for processors with RGMII support, but for STM32H7 RMII Ethernet, use a proper RMII PHY.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Aug 27, 2026 8:43 AM UTC

Hello,

A question that you need to address to Realtek

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.