Skip to main content
Nobuhide Iinuma
Associate
May 30, 2017
Question

Can 5 V tolerant pin be turned off?

Posted on May 30, 2017 at 11:26

Hi,

I am using the NUCLEO - L053R8 circuit board.

I question about 5 V tolerant function.

A pull-up resistor driven by 5 V is added to the port of PA_8.

In this case, when setting the open drain setting, 0.1 mA flows.

However, setting to input setting is 0 mA.

I want to set the current to 0 mA in the open drain setting state.

question 1

In the open drain setting, does the protection diode work?0690X00000607AWQAY.png

Question 2

Please check if my open drain setting method is correct.

It is set with mbed.

///////////////////////////////////////////

&sharpinclude ''mbed.h''

DigitalInOut Common_5(PA_8);

int main() {

while(1) {

Common_5.mode(OpenDrain);

wait_ms(2);

}

}

///////////////////////////////////////////

Thanks

#gpio #mbed #nucleo-l053r8 #5v-tolerant
This topic has been closed for replies.

6 replies

Max
ST Employee
May 31, 2017
Posted on May 31, 2017 at 04:43

Hello,

If you turn off the

GPIO, you will not get the

LOW

level state anymore...

the current you are talking about only exists when the output is set to

 

LOW

level.

When the output is set to

OD

 

HIGH

level, the current is 0.

This current only depend on the external resistor value, if you don't have speed constraint, try to increase the value to reduce the current..

the protection works because there is an internal protection device - similar to a zener diode - between the internal protection rail

V

DD_FT

 

and

GND.

The mbed configuration looks right to me...

Nobuhide Iinuma
Associate
June 1, 2017
Posted on June 01, 2017 at 02:58

Thank you for your reply.

I got very helpful.

Let me ask you a question.

It is connected to 5V with an open drain pin sandwiching a 1.5K resistor.

(It pulled up with 1.5 KΩ)

The power supply of the CPU is 3.3V.

Even if it is in the open drain state, it will flow 0.23 mA.

This is thought to be the influence of the protection diode as in MAX's mail.

I do not want current to flow through the pull-up resistor in the open drain state.

With STM32 MCU, can not you do something like this?

Thank you.
Nobuhide Iinuma
Associate
June 1, 2017
Posted on June 01, 2017 at 03:23

Supplement.

Supplement the case of INPUT setting.

The INPUT setting pin is connected to 5 V across a 1.5 KΩ resistor.

(It pulled up with 1.5 KΩ)

The power supply of the CPU is 3.3V.

In this case, the current value is zero.

It seems that the protection diode is released.

With INPUT setting, will the breakdown occur even if the pull-up resistor is connected at 5 V?

Thank you.