Skip to main content
Associate
Jul 17, 2025 9:04 AM UTC
Question

BMP581 data problem

bmp581 data problem
I'm using a BMP581 barometric pressure sensor on my custom flight computer designed for a rocket project. The altitude data I read from the sensor is not stable over time. While the sensor is in a stationary position (not moving), the altitude value sometimes slowly decreases, reaching values like -70 meters, and then slowly starts increasing again.

It doesn't immediately drop to a negative value — instead, it drifts gradually over time, showing a kind of up-and-down fluctuation. Sometimes it reaches a stable point temporarily, then begins drifting again. The environment is stable and there is no actual altitude change.

This issue does not occur when I test with last year's flight computer using the same sensor model, so I'm trying to understand whether this is a hardware-related issue (power supply, layout, noise) or if something in my software or configuration could cause it.


The first circuit belongs to this year, and the second one is from last year. The first one has the same problem even though I removed the components L8 and C31 instead of keeping them. I don't understand why. The other connections and the code are the same as last year

See less

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
Jul 17, 2025 9:27 AM UTC

welcome to the forum

 


@MertRonom9 wrote:

The first circuit belongs to this year, and the second one is from last year. The first one has the same problem even though I removed the components L8 and C31


We have no idea what these are - you need to post full details.

Please see How to write your question to maximize your chances to find a solution 

 


@MertRonom9 wrote:

I'm trying to understand whether this is a hardware-related issue (power supply, layout, noise) or if something in my software or configuration could cause it.


Have you used an oscilloscope to see if there is noise or power supply issues?

Have you used an analyser to see the comms with the sensor?

Have you tried logging the raw data?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
Principal
Jul 17, 2025 9:49 AM UTC

> I'm using a BMP581 barometric pressure sensor on my custom flight computer designed for a rocket project. The altitude data I read from the sensor is not stable over time. While the sensor is in a stationary position (not moving), the altitude value sometimes slowly decreases, reaching values like -70 meters, and then slowly starts increasing again.

As said, this sensor measures barometric pressure - not altitude. The altitudes are your interpretation.

First, I suppose you know that barometric pressure is not constant. In fact, it can vary significantly in the very same location over the day. To interpret a barometric pressure as altitude, a very recent calibration to the local pressure is essential. And essential means before every single use.

Secondly, I have dealt with the BMP280, which has a quite elaborate calibration process. I assume the BMP580 is not dissimilar.  But for a proper calibration, your measuring hardware must have reached thermal equilibrum. As it sounds, some of your boards do not - otherwise values wouldn't drift so much. Or, as noted below, the supply voltage drifts.

>The first one has the same problem even though I removed the components L8 and C31 instead of keeping them.

I have no idea what you are talking about.
If you refer to a specific board, show us the schematics, or a link to it.
Although from the component names, I don't think they can influence pressure readings in any way directly.

> This issue does not occur when I test with last year's flight computer using the same sensor model, so I'm trying to understand whether this is a hardware-related issue (power supply, layout, noise) or if something in my software or configuration could cause it.

Thus your assessment as "bug report" is very rushed.

Perhaps an electrical issue like supply voltage drift or thermal problems. Or a change in design regarding air flow direction and orientation.