Skip to main content
Associate
Jul 13, 2026 11:05 PM UTC
Solved

Biricha WDS Configuration for Synchronous Buck Converter

Hello, 

I’m writing in regards to a project that I am doing that involves a STM32G474RGT being used to control a synchronous buck converter. In this set up I plan to use Peak Current Mode Control, which I found was supported by Biricha’s WDS software. As a result I configured my HRTimers and ADC and Comparators like the guides that I found online, mainly the step by step setup on the Biricha Youtube Channel. However, upon opening up the software, I noticed that the circuit tab for the buck setup would only show up as an asynchronous buck, using a diode instead of 2 N-Channel mosfets. Is there anyway to configure the software to use a synchronous buck topology? 

Brian

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 15, 2026 9:54 AM UTC

Hello ​@bguan08 and welcome to the ST community,

Better to ask that question to Biricha (over contact us link) as it’s not a ST solution.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 15, 2026 9:54 AM UTC

Hello ​@bguan08 and welcome to the ST community,

Better to ask that question to Biricha (over contact us link) as it’s not a ST solution.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
bguan08Author
Associate
Jul 16, 2026 2:51 AM UTC

Ah ok, sorry for posting this in the wrong location. Thanks for replying though!