Skip to main content
michal_ca
Associate II
Oct 7, 2019 2:01 PM UTC
Question

BDMA 50ns offset between Clock (LPTIM2 PWM) and 16bit GPIOE.

Hi all,

I working on parallel synchronous transmission. I am using LPTIM2 as clock (PWM) and GPIOE as data bus. It is working with BDMA but here is 50ns offset between Clock and data no matter what frequency I setup. Please see pictures below 84kHz and 8MHz.  So I would like to eliminate 50ns offset between clock and data.

I trying to make synchronisation at falling edge of CLK. And my goal is reach 16MHz.

It is even possible with STM32H7 ?

Current configuration STM32H743, 400MHz, SW4STM32, HAL

Thank you

Michal

0690X000009jzrbQAA.jpg

0690X000009k06MQAQ.jpg

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
Oct 7, 2019 5:06 PM UTC

Is this a timer-triggered DMA from memory to GPIO?

Surely, there's some propagation/resynchronization time from timer to DMAMUX, within DMAMUX, from DMAMUX to BDMA; then BDMA performs arbitrration, loads the value from the source memory and finally outputs to the GPIO, again all these processes take some time to accomplish.

You can compensate somewhat by triggering the BDMA from a different channel of the timer, slightly skewed to the one which outputs the "clock".

Note, that in a real program, not only a fixed delay is imposed, but due to potential conflicts within BDMA and on the source/destination buses of the DMA, this time might be increased at certain moments, resulting in jitter.

JW

michal_ca
michal_caAuthor
Associate II
Oct 8, 2019 11:42 AM UTC

Yes a timer-triggered BDMA from memory SRAM4 to GPIO

Sure I understand that all these operation take some time, however the example AN4666 with STM32F4 and STM32L4 work without resynchronization.

waclawek.jan
Super User
Oct 8, 2019 2:31 PM UTC

And what is chapter 1.2.2 Data and clock alignment consideration talking about, then?

JW