Skip to main content
Visitor II
Nov 8, 2025 2:07 AM UTC
Solved

Are the TLV2372's surroundings and pin connections correct ?

STM32F030F4P6TR'nin PA5 pininde PWM araştırmaları. TLV2372ID ile 0-10V analog çıkış elde etmeyi planlıyorum. Devre şemasının doğru olması gerekiyor. TLV2372'nin sınırları ve pin bağlantıları doğru mu?

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 9, 2025 12:50 PM UTC

English is not my native language either, but it is the language of communication defined by the community, which is why I am responding in English here.

For 0...10V, an opamp with approximately three times the gain is required (3.03, to be precise) if you have a VCC of 3.3V. According to the connection diagram, you have wired it correctly, although a drawing of opamps with a classic triangle would be clearer and better readable for the supporters here.

Please note: even though the TLV2372 is an RRIO opamp, it will output a significant output voltage of approx. 200mV at a VDD of 12V and very low input voltages close to 0.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 9, 2025 12:50 PM UTC

English is not my native language either, but it is the language of communication defined by the community, which is why I am responding in English here.

For 0...10V, an opamp with approximately three times the gain is required (3.03, to be precise) if you have a VCC of 3.3V. According to the connection diagram, you have wired it correctly, although a drawing of opamps with a classic triangle would be clearer and better readable for the supporters here.

Please note: even though the TLV2372 is an RRIO opamp, it will output a significant output voltage of approx. 200mV at a VDD of 12V and very low input voltages close to 0.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.