Skip to main content
Karan 123
Senior
Dec 28, 2021 4:39 PM UTC
Question

AN4894 : Struggling with Integration X-CUBE_EEPROM with Existing (.ioc) Project.

Hi,

I am working on STM32G071RB MCU

This is continuation topic of below Post :

https://community.st.com/s/question/0D73W000001N7XW/stm32g0-flash-as-eeprom?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&s1uid=0050X000007vw7K&emtm=1640084190435&fromEmail=1&s1ext=0

I have read AN4894 Application note EEPROM emulation techniques and software for STM32 microcontrollers Already Copied EEPROM_Emul to Existing Project..

How to integrate X-CUBE-EEPROM for existing .ioc project ?

Why I am getting Errors (After Removing Space as in another Post)?

--

Karan

This topic has been closed for replies.

1 reply

TDK
Dec 28, 2021 9:26 PM UTC

This works better if you show the errors you're getting.

If it's still the "No such file or directory" error, then the compiler can't see the file. Ensure the path is correct. Ensure the file exists. I suppose it's possible the program lacks permissions to that directory.

I would suggest using a relative path rather than an absolute one and ensure the directory the file is in is within the list of include directories.

"If you feel a post has answered your question, please click ""Accept as Solution""."