Skip to main content
Brother Theo
Associate III
May 21, 2018 4:46 PM UTC
Question

Add file to system workbench project

Posted on May 21, 2018 at 18:46

How do I add an external file to a system workbench project? I've done it before but the method I thought I used didn't work this time. What I did was copy the file into the SRC folder of the project, then open the project and open the new file. That didn't work. So how does one do this?

#add-external-file #system-workbench
This topic has been closed for replies.

3 replies

John Fitter
Associate II
May 22, 2018 12:21 AM UTC
Posted on May 22, 2018 at 02:21

Using Eclipse I just drag the file and drop it on the project exactly where I want it.

AvaTar
Senior III
May 22, 2018 7:28 AM UTC
Posted on May 22, 2018 at 07:28

Except this Drag-and-Drop method, the file/project import is not intuitive at all.

Find a generic Eclipse tutorial, perhaps the System Workbench has even  a useful help.

Brother Theo
Associate III
May 22, 2018 5:48 AM UTC
Posted on May 22, 2018 at 07:48

I figured it out. In the project explorer at the top of the tree right click on the project name then click the refresh menu item.