Skip to main content
PaoloValentino
Associate
Jul 16, 2021 6:14 AM UTC
Solved

255 as response to eeprom

Hi,

I'm trying to write and read to/from M24512-R EEPROM.

Seems that everything is fine writing and reading because HAL return is HAL_OK, but allways I've reading 255 value.

My code:

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_I2C2_Init();
 MX_USART1_UART_Init();
 MX_USART3_UART_Init();
 MX_ADC1_Init();
 MX_TIM4_Init();
 /* USER CODE BEGIN 2 */
 const uint8_t num_data = 5;
 uint8_t datos[num_data];
 uint8_t datos_in[num_data];
 uint8_t number = 100;
 HAL_StatusTypeDef escritura = 4;
 HAL_StatusTypeDef lectura = 4;
 uint32_t error =0;
 HAL_I2C_StateTypeDef state = HAL_I2C_STATE_READY;
 /* USER CODE END 2 */
 for (int i = 0; i<=num_data-1; i++)
 {
 	 datos[i] = 0;
 }
 for (int i = 0; i<=num_data-1; i++)
 {
 	 datos_in[i] = 0;
 }
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 for (int i = 0; i<=num_data-1; i++)
 {
	 datos[i] = number - i*2;
 }
 
 HAL_GPIO_WritePin(WP_EEPROM_GPIO_Port, WP_EEPROM_Pin, GPIO_PIN_RESET);
 escritura = HAL_I2C_Mem_Write(&hi2c2, ADDMEMORY, ADDRDATA, 2, datos, num_data, 1000);
 if (escritura !=HAL_OK)
 {
	 state = HAL_I2C_GetState(&hi2c2);
	 error = HAL_I2C_GetError(&hi2c2);
 }
 HAL_GPIO_WritePin(WP_EEPROM_GPIO_Port, WP_EEPROM_Pin, GPIO_PIN_SET);
 //HAL_I2C_Mem_Write(halI2C, ID esclavo, dir_memoria_inicial, tamaño palabra en bits, buffer a guardar, cantidad datos, tiempo espera);
 uint8_t went_well = 0;
 bool test_passed = false;
 HAL_Delay(100);
 lectura = HAL_I2C_Mem_Read(&hi2c2, ADDMEMORY, ADDRDATA, 2, datos_in, num_data, 1000);
 for (int i=0; i<=num_data-1; i++)
 {
	 if (datos[i] == datos_in[i])
	 {
		 went_well ++;
	 }
 }
 while (1)
 {
	/* USER CODE END WHILE */
 
	/* USER CODE BEGIN 3 */
 
 
 }
 
 /* USER CODE END 3 */
}
 
/* I2C2 init function */
void MX_I2C2_Init(void)
{
 
 hi2c2.Instance = I2C2;
 hi2c2.Init.ClockSpeed = 100000;
 hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c2.Init.OwnAddress1 = 0;
 hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c2.Init.OwnAddress2 = 0;
 hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c2) != HAL_OK)
 {
 Error_Handler();
 }
 
}

And attached oscilloscope images:

WRITE COMMAND

0693W00000CzlwvQAB.pngREAD COMMAND

0693W00000Czlx0QAB.png 

I've checked all pins, VCC and E0-E2 are connected to GND.

Any idea of what I'm doing wrong?

Thanks in advantage.

This topic has been closed for replies.
PaoloValentino
PaoloValentinoBest answer
Associate
Jul 19, 2021 10:05 AM UTC

Fixed it writting a HAL_Delay(10) after HAL_I2C_Mem_Write(). Seems WRITE pin wasn't in high level enough time to carry out write process.

1 reply

PaoloValentino
PaoloValentinoAuthorBest answer
Associate
Jul 19, 2021 10:05 AM UTC

Fixed it writting a HAL_Delay(10) after HAL_I2C_Mem_Write(). Seems WRITE pin wasn't in high level enough time to carry out write process.