Skip to main content
smshenoy
Associate
May 9, 2008 11:27 AM UTC
Question

xti to arm7

Posted on May 09, 2008 at 13:27

xti to arm7

This topic has been closed for replies.

2 replies

smshenoy
smshenoyAuthor
Associate
May 7, 2008 5:19 PM UTC
Posted on May 07, 2008 at 19:19

I have configured the ARM7 for external interrupts on P2.8

I am toggling a i/o P2.12 in the interrupt handler (to indicate that it is getting executed).

Whenever the interrupt is generated from the external hardware the led associated with P2.8 goes low (typically lit or high). But the led on P2.12 does not toggle. I looked through the configuration and they looked alrite. Also the vector table. The code snippet is attached here. Any leads would be appreciated.

// Enable XTI and GPIO2 clocks on APB2

APB_ClockConfig(APB2, ENABLE, GPIO2_Periph | XTI_Periph);

// XTI configuration

XTI_Init();

XTI_LineModeConfig(XTI_Line2, XTI_FallingEdge);

XTI_LineConfig(XTI_Line2, ENABLE);

XTI_ModeConfig(XTI_Interrupt, ENABLE);

// Configure XTI IRQ channel

EIC_IRQChannelPriorityConfig(XTI_IRQChannel, 4);

EIC_IRQChannelConfig(XTI_IRQChannel, ENABLE);

EIC_IRQConfig(ENABLE);

GPIO_Config(GPIO2, 0x0001 << 0x08, GPIO_IPUPD_WP);

smshenoy
smshenoyAuthor
Associate
May 9, 2008 11:27 AM UTC
Posted on May 09, 2008 at 13:27

Some more information.

I see that the CICR and CIPR are set even before reaching my while loop. I made sure they are cleared using the EIC_Init(); Even then the registers get set for the channel I am intersted in just before entering the while loop.

Any leads why this might be happening?