Skip to main content
Associate
May 4, 2024
Question

WS2812B with STM8s003

Hello, I have bought an STM8s003 board and would like to use it to control ws2812B LEDs. But the libraries I have used with other controllers e.g. FastLED are not compatible with the STM8s003. Do you have any idea how I can solve this? I would prefer to be able to continue using the Arduino IDE as before.

    This topic has been closed for replies.

    7 replies

    Erik1Author
    Associate
    May 4, 2024

    I have found a librarie but one date is lost:

    https://github.com/thielj/FastLED-STM8/tree/master

    FastLED/platforms/stm8/hal/iostm8.h

    Andrew Neil
    Super User
    May 7, 2024

    @Erik1 wrote:

    I have found a librarie but one date is lost:

    https://github.com/thielj/FastLED-STM8/tree/master

    FastLED/platforms/stm8/hal/iostm8.h


    Did you follow the instructions for getting help with that library?

    AndrewNeil_0-1715087399417.png

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Peter BENSCH
    ST Technical Moderator
    May 7, 2024

    Welcome @Erik1, to the community!

    Since it is a library from Github (forked the project from FastLED) that has nothing to do with STMicroelectronics, you would have to ask the developer there, but he doesn't seem to want to be approached. I suspect that one of the files STM8S003F3.h or STM8S003K3.h needs to be copied to stm8/hal and renamed to iostm8.h.

    Hope that helps?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Andrew Neil
    Super User
    May 7, 2024

    @Erik1 wrote:

     Do you have any idea how I can solve this? I would prefer to be able to continue using the Arduino IDE as before.


    Three options:

    1. Understand how the existing libraries (eg FastLED) work, and port that to STM8;
    2. Find a library for STM8;
    3. Create STM8 code by working from first principles:
      http://www.8052mcu.com/forum/read/160143 

     


    @Erik1 wrote:

    I would prefer to be able to continue using the Arduino IDE as before.


    Seems there is some Arduino support for STM8:

    https://www.google.com/search?q=Arduino+core+available+for+STM8 

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 7, 2024

    Does it have to be WS2812B ?

    eg, APA102 or SK9822 use a standard SPI connection - so you wouldn't have to mess about with bit-banging the proprietary critical timing of WS2812B ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Michal Dudka
    Lead
    May 14, 2024

    Regardless of what environment or microcontroller you use there is one elegant solution - use SPI MOSI signal (ignore SCK). Imagine you have SPI running at 8MHz. When you send value 0b01110000 SPI generate positive pulse with duration 3*125ns (375ns) and followed by negative value with duration (5)*125ns(625ns). Which is legal WS2812 bit with value "0". If you want to send "1" bit, then you simply send value 0b01111100 (625ns in High + 375ns in Low). By this method you can overcome problems with precise "delays" and moreover you can also pack two WS2812 bits into one SPI byte (!). For example 3MHz SPI can generate 0b0100  (333ns pulse, 999ns space) + 0b0110  (666ns pulse, 666ns space).

     

    Andrew Neil
    Super User
    May 14, 2024

    Indeed - have done this on an nRF chip!

    Same approach can also be used for some other "bit-bang" applications; eg, it has been done with the Maxim/Dallas 1-Wire(TM) protocol ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.