Skip to main content
Philipp Krause
Senior II
July 21, 2022
Question

Why use non-free compilers (Cosmic, etc) instead of SDCC?

I wonder why some developers choose non-free compilers (IAR, Cosmic, Raisonance, etc) instead of the Small Device C Compiler (SDCC) when targeting the STM8.

    This topic has been closed for replies.

    1 reply

    Michal Dudka
    Lead
    July 23, 2022

    I am not representative example (i do only two or three small projects with STM8 per year). But i've choosen Cosmic because it was simple to set up and run toolchain on windows (about one day with zero STM8 knowledge to running program with IRQs etc).