Skip to main content
VSchu.1
Associate II
July 20, 2021
Question

Why can't I use UART1 and ADC1 together?

Hi. I made a code that uses ADC1 in single conversion mode and UART in asynchronous mode.

But when I do the ADC1_Init() for some reason the RX interrupt of the UART doesn't work, if I don't use the ADC1 it works normally. Can someone help me?

Peripheral Settings

CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1); 

GPIO_DeInit(GPIOA); // GPIOA reset

GPIO_DeInit(GPIOB); // GPIOB reset

GPIO_DeInit(GPIOC); // GPIOC reset

GPIO_DeInit(GPIOD); // GPIOD reset

GPIO_DeInit(GPIOE); // GPIOD reset

//SAIDAS

GPIO_Init(DIG1, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(DIG2, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(DIG3, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGA, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGB, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGC, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGD, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGE, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGF, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(SEGG, GPIO_MODE_OUT_OD_LOW_SLOW);

GPIO_Init(SEGDP, GPIO_MODE_OUT_OD_LOW_SLOW);

GPIO_Init(DIGITALOUT, GPIO_MODE_OUT_PP_LOW_FAST);

//CONFIGURACAO EEPROM

FLASH_SetProgrammingTime(FLASH_PROGRAMTIME_STANDARD);

 

//BASE DE TEMPO 1MS TIM4

TIM4_TimeBaseInit(TIM4_PRESCALER_128, 124);

TIM4_ClearFlag(TIM4_FLAG_UPDATE);

 TIM4_ITConfig(TIM4_IT_UPDATE, ENABLE);

 TIM4_Cmd(ENABLE);

//ADC CONFIG

ADC1_DeInit();

ADC1_Init(ADC1_CONVERSIONMODE_SINGLE, 

        ADC1_CHANNEL_4,

        ADC1_PRESSEL_FCPU_D4, 

        ADC1_EXTTRIG_TIM,DISABLE, 

ADC1_ALIGN_RIGHT, 

        ADC1_SCHMITTTRIG_ALL,DISABLE);

ADC1_ScanModeCmd(ENABLE);

ADC1_Cmd(ENABLE);*/

 //CONFIG UART1 CALIBRACAO E *****

UART1_DeInit();

UART1_Init((uint32_t)9600, 

UART1_WORDLENGTH_8D, 

UART1_STOPBITS_1, 

UART1_PARITY_NO, 

UART1_SYNCMODE_CLOCK_DISABLE, 

UART1_MODE_TXRX_ENABLE);

UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);

enableInterrupts();

RX reading (only works if ADC is not started)

 INTERRUPT_HANDLER(UART1_RX_IRQHandler, 18)

 {

 

buffer[counter] = UART1_ReceiveData8();

 counter++;

if(counter > 10)UART1_ITConfig(UART1_IT_RXNE_OR, DISABLE);

 

}

ADC input reading

ADC1_StartConversion();

while(ADC1_GetFlagStatus(ADC1_FLAG_EOC) == RESET);

voltageAverage[averageCounter] = (unsigned int)ADC1_GetBufferValue(ADC1_CHANNEL_4);

ADC1_ClearFlag(ADC1_FLAG_EOC);

Thanks

    This topic has been closed for replies.

    1 reply

    VSchu.1
    VSchu.1Author
    Associate II
    July 21, 2021

    Can solve the problem, if someone has the same problem.

    The pins I'm using as serial RX and TX are the analog inputs Ain5 and Ain6, so I had to modify the following registered:

    ADC1->TDRL &= 0b10011111;