Skip to main content
s1975
Associate II
Aug 1, 2013 9:56 AM UTC
Question

whether there are libraries for STM8 periphery? (assembler)

Posted on August 01, 2013 at 11:56

whether there are libraries for STM8 periphery? (assembler)

I didn't find if at someone is, report the link, please.

    This topic has been closed for replies.

    4 replies

    s1975
    s1975Author
    Associate II
    Aug 1, 2013 9:57 AM UTC
    Posted on August 01, 2013 at 11:57

    STVD assembler

    fggnrc2
    Associate III
    Aug 1, 2013 10:04 AM UTC
    Posted on August 01, 2013 at 12:04

    The hardware peripheral include files are stored under the root directory of your STVD installation, i.e. inside C:\Program Files\STMicroelectronics\st_toolset\asm

    s1975
    s1975Author
    Associate II
    Aug 1, 2013 10:11 AM UTC
    Posted on August 01, 2013 at 12:11

    more correctly, for example i2c library, etc., so that it would be possible to use record and reading function, as for C

    fggnrc2
    Associate III
    Aug 1, 2013 11:22 AM UTC
    Posted on August 01, 2013 at 13:22

    Sorry, there is no assembler library for using a STM8 peripheral.

    If you want one, you could compile the STM8 standard peripheral library and use the compiler assembler output.

    You can also ''call'' the library C functions from your assembler code if it meets the calling convention of the C compiler, but it's easier to ''translate'' the C algorithm in an assembler one starting from the assembler output of the compiler...