Skip to main content
hkavi.695
Associate II
April 25, 2021
Question

where to find examples code for ST10 MCUs?

Hi there

I've recently started working with st10f275 microcontroller. I am totally confused. I can't event find its datasheet! which compiler, ide, programmer should I use?

Could anyone guide me?

Thanks in advance.

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
April 25, 2021

>>I've recently started working with st10f275 microcontroller.

Bit late to the party there, isn't this obsolete already?

Based on the old C166 designs

Try related data sheets https://www.st.com/en/automotive-microcontrollers/st10f276e.html

https://www.keil.com/c166/

https://www.tasking.com/support/c166-st10-c-compiler-toolset-support

https://cosmic-software.com/st10.php

>>Could anyone guide me?

Is this a well paid role?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
hkavi.695
hkavi.695Author
Associate II
April 25, 2021

Thanks for the comment. I'm using Keil and S10flasher. this is the report of S10flasher, but It doesn't work. I don't know how to debug my code.

*FILE INFO FOR FILE:Hello.H86

Size = 1315 bytes.

Programming time = 2 s.

Block(s): 

*Set com parameters:COM3, 9600 bauds-->OK

*LOAD MONITOR-->OK

*Lost of monitor communication

Reset the board and reload the monitor

Tesla DeLorean
Guru
April 25, 2021

Lacking the type of hardware debug pods of modern times one might need to consider GPIO pins and UART output to report internal state information, and add monitor type functionality (ie command line debug running within the device) like MON166

Or the use of emulators. where the chip is replaced by hardware that basically spoofs that of the target.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..