Skip to main content
Philipp Krause
Senior II
Sep 19, 2018 7:01 PM UTC
Question

When will STLINK-V3 and MB1440 become available?

TN1235, released this month has some basic information on the new STLINK-V3 (which already can be ordered at some distributors, but lead times are long, and where there are pictures they show the older ST-LINK/V1)

According to TN1235, for the SWIM interface (and thus for using STLINK-V3 with STM8) one needs some adapter board called MB1440. I found no mention of MB1440 outside of TN1235.

When will STLINK-V3 and MB 1440 become available?

Philipp

This topic has been closed for replies.

5 replies

martonmiklos
Senior
Sep 27, 2018 1:49 PM UTC
S C
ST Employee
Sep 28, 2018 10:56 AM UTC

More information will come mid-october​

Philipp Krause
Senior II
Oct 2, 2018 8:06 PM UTC

I received a note from someone who bought it at Mouser. Apparently, the STLINK-V3SET comes with the MB1440 included.

Philipp

Philipp Krause
Senior II
Oct 3, 2018 8:42 AM UTC

Images and link to USB data on a blog (not mine):

http://users.atw.hu/balubati/blog/index.php?entry=entry181002-114748

Philipp

martonmiklos
Senior
Oct 5, 2018 12:55 PM UTC

@S C​ 

It is a nice piece of hardware, with excellent capabilities!

Do you know if the protocol for the direct access of the USB-CAN, USB-I2C, USB-SPI will be published?

Documentation to the standard programming capabilities JTAG, SWD, SWIM would be very useful as well. (If not we have to reverse engineer it ;))