Skip to main content
nanuradha
Associate III
Sep 12, 2006 4:01 AM UTC
Question

What is the purpose of SRAM_SIZE option in STR91 series

Posted on September 12, 2006 at 06:01

What is the purpose of SRAM_SIZE option in STR91 series

This topic has been closed for replies.

2 replies

kais
Associate
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi anuradha,

After reset the size of the on-chip SRAM is limited to 32K .among STR9 features :the configurable size of its SRAM (32K, 64K,96K).So it depends on the complexity of your application to select a large size : Application including RTOS, TCP/IP stack…

Regards

Eris.

nanuradha
nanuradhaAuthor
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

In the reference manual SRAM_SIZE option is there.In what application is that useful.Is there any restriction depending on SRAM size on other features.

Regards

Anuradha.