Skip to main content
cmao
Associate
Dec 19, 2004 8:57 AM UTC
Question

what is the maximum supply voltage for analog circuits (maximum AVcc)?

Posted on December 19, 2004 at 09:57

what is the maximum supply voltage for analog circuits (maximum AVcc)?

This topic has been closed for replies.

2 replies

cmao
cmaoAuthor
Associate
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

Our analog input ranges from 0 to 4V, so my question is:

can I use the ADC in uPSD3354DV ? In other words, I'd like to set reference voltage Vref = 4.096 V, supply analog circuits with AVcc = 5V, MCU Module Vcc= 3.3V, and PSD module Vdd=3.3V, is this setting feasible?
daxenberger
Associate
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

Hi,

AVref maximum is 3.6V! So you cannot use a higher voltage reference!

You have to scale down your input voltage to a range that will not damage the MCU.

Regards,

Stefan