Skip to main content
xiao
Associate
Jun 1, 2006 11:54 AM UTC
Question

what is the maximum pin sink current, IOL??

Posted on June 01, 2006 at 13:54

what is the maximum pin sink current, IOL??

This topic has been closed for replies.

2 replies

hanwayh
Associate
May 17, 2011 10:10 AM UTC
Posted on May 17, 2011 at 12:10

IOL is 10 mA at VOL = 0.6V for port 4 and is 8 mA for Port A, B, C, and D. However, the total operating current in Turbo mode is about 79 mA (5V) or 63 mA (3.3 V).

Driving LED with 20 mA is too much for the MCU.

han-way

xiao
xiaoAuthor
Associate
May 17, 2011 10:10 AM UTC
Posted on May 17, 2011 at 12:10

please help to find out the upsd3354 maximum pin sink current limit, IOL. I could not find it out from the data sheet.

Could I directly use a GPIO pin to sink about 25mA current, for example, to drive a LED?